Part Number: TX7332EVM
I want to reduce the frequency of the TR switches from 1kHz to somewhere around 250Hz. Previously I asked how to do this on the forums and was told to "remove R139 resistor on the TX7332 EVM and apply an external SYNC signal on U10 pin #3 using AWG." However, checking the datasheet and probing the pins shows that pin #3 is always held high at 1V and pin #2 is the one with the pulse. Is it correct then that pin#2 is where I should apply the SYNC signal and not pin #3? And is this SYNC signal just a short pulse?
Also, instead of modifying the hardware, is there a way to modify the CPLD's programming to change the sync pulse rate while still using the GUI without issues?