Part Number: DAC8760
HI,
I have some question in setting DAC8760 as below:
Dac8760 sets the output current of 4 ~ 20mA and the actual output current of 9 ~ 12mA.
The register configuration has been confirmed to be OK by reading the register.
Do you need to do other configuration on the software? Is there a problem with the hardware design?
Code:
Dac8760 ﹐ write (w ﹐ addr ﹐ reset, 1); / / reset all registers
Dac8760 write (W addr Ctrl, (1 < < 12) | 0x05); / / configure output current
Dac8760 ﹣ write (w ﹣ addr ﹣ data, 0xFFFF); / / output 20mA
Schematic as below:
thanks,