This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS42LB69: Two ADS42LB69s Synchronization

Part Number: ADS42LB69

Hello,

 

In order to align two ADS42LB69 outputs, SYNCINN/P have to be used, even the input clock divider is bypassed (divide-by-1)?

Or if CLKINP/N phases are aligned at two ADS42LB69s, no need to use SYNCINN/P when the input clock divider is bypassed?

 

Best regards,

 

K.Hirano