Part Number: ADS8866
Hi,
I want to use the ADS8866 with a reference voltage of 3.3V.
To get a good Resolution the expected voltage is in the range from 0V-3V.
If a fault happens the voltage can reach 5V. I protect the Inputs of the ADS8866 with a series resistor (Figure 51) of 1k so the expected current in the Input Pin will be less than 2mA.
In the datasheet I find a value "Input current to any pin expect supply Pins <10mA". Is this value also valid for the AINP & AINN Pins ?
Kind regards