This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS131E08: Using both internal and external volt reference

Part Number: ADS131E08

Hi,

Are there any settings in the ADC which would allow the use of the internal voltage reference while there is an external voltage reference connected as well? How would I go about doing that?

Best,

Adam

  • Adam,

    In order to use both the internal and external voltage reference, I think you would need some sort of external switch to disconnect the external reference. A diagram of the reference connections is given in the datasheet in Figure 28.

    With those connections, any external reference would need to be disconnected before using the internal reference.

    Joseph Wu