Hello.
I have previously asked that there is a problem with continuously IQ measurements.
link : e2e.ti.com/.../881585
The answer was then asked to see the Archiving Deminist phase in IQ Mode section on the datasheet.
I looked it up and read it, but I can't understand it.
Can you explain it in detail?
The picture below shows the results obtained by continuous measurements.
The order is the same as 8 kHz (I,Q) - 16 kHz (I,Q) - 32 kHz (I,Q) - 64 kHz (I,Q) - FWR, programmed to repeat.
At 8 kHz, I and Q values are constant even when measured repeatedly.
However, at other frequencies, the change in Q value was particularly significant.
Help me.