Part Number: AMC1210MB-EVM
Other Parts Discussed in Thread: AMC1210,
Hello,
I am using AMC1210 Eval board with my ADC device ADuM7701. The ADuM7701 dont have internal clock and the maximum clock frequency of ADuM7701 is 20MHz. The clock of AMC1210 is 32MHz. As per the data sheet it is saying that we can divide the clock and apply to modulator.
My question is, if I want to use AMC1210 eval board clock (16MHz) to ADuM7701, what mode need to be selected in Eval tool? I need these changes in current shunt mode.
Can I do these changes in Eval tool in current shunt mode?
Thank You
Regards,
Bhargav Pendurthi