Part Number: ADC08060
The datasheet says this part operates from 20MSPS to 70MSPS.
Is there any reason I can't operate this slower with a clock rate of 10MHz?
And does the output Data stay constant and can be read asynchronously at anytime?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ADC08060
The datasheet says this part operates from 20MSPS to 70MSPS.
Is there any reason I can't operate this slower with a clock rate of 10MHz?
And does the output Data stay constant and can be read asynchronously at anytime?
Hi William,
I believe the reason that operation is limited to 20MSPS is to guarantee data sheet performance specifications. My hunch is that the part will operate similarly in terms of conversions to output data at a slightly lower clock rate, but I cannot say for sure.
The output data bits (D0 - D7) are synchronous to the sample clock, but there is a delay (t_OD) between the edge of the sample clock and edge of the corresponding data bits. See timing diagram on page 17.
Best Regards,
Dan
Hi William,
I have done some testing on the ADC08060EVM, and have the following results.
10 MSPS: 1 MHz input (band-pass filter): ~46 dBFS SNR and ~61 dBFS SFDR
60 MSPS, 1 MHz input (band-pass filter): ~46 dBFS SNR and 60 dBFS SFDR
Best Regards,
Dan