This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC8871: Using as single analog supply device

Part Number: DAC8871


Hi,

I want to use the DAC8871SPW IC for an application with 0-15V variations.

So Is it correct to ground the VSS and VREFL-F & VREFL-S pins to AGND?

The VDD connection will be with 3.3V and VCC and VREFH-F,VREFH-S are shorted together.

Can anyone please help me with this.

Thanks & Regards,

Nanjunda M