Other Parts Discussed in Thread: LMK04828,
Have 3rd party custom hardware with a LMK04828 used to source the device and SYSREF clocks for a ADS54J60. Having troubles with SPI communication. Following the initialization sequence as noted in table 75 with one notable difference. The hardware reset does not comply with the datasheet. The reset pin starts to go high with the power supplies ramping up then goes low before the supplies reach their nominal voltage. Guessing the invalid hardware reset may be causing the SPI communication issue.
Is the write of address 0x0000 to 0x81 truly an equivalent to a hardware reset?
Regards, Gary