This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV2541: MAX SCLK value by VDD

Part Number: TLV2541

Hi, Staff

Please ask questions in Table1 of TLV2541 Datasheet (SLAS245E) page8.

CS control only (TLV2541 only)
: For SPI interface VDD = 2.7V → 10MHz and VDD = 4.5V → 15MHz.

I want to know what this means.
Q1:10MHz when 2.7V ≦ VDD > 4.5V
Is it 15MHz when 4.5V ≧ VDD ?

Q2:What is the Data Throughput with a TYP value of VDD=3.3V?

best regards
cafain