Part Number: ADS7828
Sometimes the AD7828 appears to latch up in a state where the digital output for all channels does not match the apparent input. For example, a channel connected to an RTD has an input voltage corresponding to a temperature in the range of 19 - 25 degrees C (which corresponds to the actual temperature in the system), but the digital output for that channel corresponds to temperature of -80 degrees C. This state persists until the system is power-cycled.