Other Parts Discussed in Thread: OPA320, OPA192
Dear Support,
I need driving the ADS1672 with a single-ended signal, 4Vpp from a low-noise
voltage amplifier, while keeping the ADC specs.
The voltage amplifier has low output impedance (about 300 Ohm) and it can not drive
a load lower than 10k.Ohm. Required BW is 250Khz. Power consumption is not an issue,
The ADS1672 will be used to analyze 1/f noise in material science tests, so
the 1/f noise of any preamp/driver should be as low as possible. Its current noise, is not an issue,
due to the low output impedance of the amplifier. However, Voltage noise could be a problem.
Could you please suggest me the best front-end (driver/circuit). In the ADS1672 datasheet I only found a scheme
(Fig.41) with a single-ended signal referenced to CM and not to GND.
Thank you for your help.
Kind Regards,
Alberto