Hello;
I want to know whether I can use this IC as True diff.
For example, I will measure two different value and I want to subtract the negative ınput (ch1)from the positive input(ch2) I mean, can I read the value CH0 - CH1
Signal information
CH0: 0V to 2V
CH1: 0V to 2V
Both of these value can change anytime within these parameters I always want to read the value of CH0-CH1