This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC60501: DAC60501M and DAC60508M

Part Number: DAC60501

DAC60501M and DAC60508M

We shall a new series of low cost single and multichannel ±10V outputs.

During power up the above PN's will reset to mid voltage.

This will then be 1.250V during first power up.

If we then program the output range scale to be from 0V to 5V will the next reset to mid voltage after an ON/OFF/ON power cycle be 2.500V or will it always be 1.250V after a power ON/OFF/ON cycle.

Regards

Jørgen