Part Number: ADS8688EVM-PDK
Other Parts Discussed in Thread: ADS8688, ADS8664, ADS8668, ADS8674, ADS8678, ADS8684, , ADS8688A
Hi,
I have installed the "ADS8688EVM GUI" software.
In the installation itself the device installation wizard announced it can't complete the device driver installation.
GUI was working for a while but after some time stopped to connect (without any hardware change )and now not able to connect the evaluation board with the PC: "sdcc interface not detected"
The evaluation board is connected to the PC win10 through USB, the green led D5 is on and the green led D2 is blinking, as it is said in the manual.
When i try to connect the ADS86XX EVM to hardware a message "SDCC Interface not detected" is shown.
PC reffered the device as generic bulk device
According similar cases here in the forum
and according
https://www.ti.com/tool/ADS8688EVM-PDK links in support section
it's seem to me that I met the same driver issue with PC win 10 ?
can you please share the Windows10 pro version driver to me with install instruction on how to updated the driver
Thanks.in advnce,
BR
ilay