Part Number: DAC5578
Other Parts Discussed in Thread: DAC53401
Hi expert,
Customer is seeking for DAC with below sepc:
- Channel number : >= 4 channel
- Output type: current or voltage both OK, for both type, need DAC can sink or source current. For the current output, the sink/source current need be >= 200uA. For the Voltage output type, the max output voltage need > 1.25V.
- Output need be in High-impedance after power on reset
- I2C interface
- 8 bit would be enough for the margin usage
- Low cost
Would you please help recommend?