Part Number: ADS114S08
Hello,
I was given a ADS114S08 that uses an external 2.5V connected to REFP0, which i figured is redundant since it already has an internal reference. A new application rose up, and I switched out the external reverence for one that supplies 3V. When testing the ADC by applying external voltages to the input, i get about a 0.5V offset from what I am applying.
I'm wondering if the ADC is still using the 2.5V reference. Is the ADC defaulted to using the internal reference? Is there an extra step I missed when using an external reference? Any assistance would be appreciated.
Best Regards,
Miguel Partida