This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC3441: Setup and hold times for 20 MSPS (2 wire mode)

Part Number: ADC3441


Hi,

In the datasheet for the device it lists in Table 1 setup and hold times for a selection of sampling frequencies (for 2 wire mode), but this does not include values for 20 MSPS. Do I need to use the values listed for 25 MSPS, or is it safe to extrapolate values for 20 MSPS? Using the worst case ratio between the minimum values and bit clock period for the sample rate I get 2.5 ns setup and 2.65 ns hold time for 20 MSPS. Is this a valid approach?

Thanks,

Ben