Part Number: ADS1298
Hi there,
I am working on a project with the ADS1298, and reviewing the datasheet I have some doubts with the power supplies.
First, two types of sources are specified, analog (AVDD) and digital (DVDD) both suggested with different voltages. Then, you have the option of feeding the circuit in a "unipolar" or "bipolar" way, in my case it would be a unipolar way and this is where I have some questions:
1) Is it necessary to use two sources to power the ADS1298?
2) Can I power the ADS1298 with a digital source and make AVDD = DVDD? and therefore AVSS = AGND and supply the circuit with 3.3v?
3) What is the specific difference between the analog and digital source in this case?
To guide a little about what I want to do, it is a cardiac signal monitoring system, using the ADS1298 and a microcontroller (ESP32), initially I would only use 2 channels of the ADS1298 (RA-LA-LL) but in the future, after carrying out some tests, I intend to increase the number of channels and electrodes, that is why it is the choice of the ADS1298.
Your answers would help me a lot to carry out my project and that it works correctly.
Thank you
Rodrigo Beltrán.