Other Parts Discussed in Thread: ADS1248, ADS1247, OMAP3530
As per a previous post I plan to use an ADS1248 for an upcoming project integrating an accelerometer and gyro but at very low variation and sampling rates. I just have a few questions regarding the pin setup before finalising my schematic.
1. I do not require to turn the unit on/off or control the sampling, we will just be constantly recieving data from the sensors. In this instance do we require DRDY or START pins and if not should they be tied or left floating.
2. We have DVDD @ 3.3v and AVDD @ 5V, I have looked through the data sheet and am still just a little unsure regarding the Vref. I have VREFOUT and VREFCOM connected with a cap and VREFCOM to ground. The analog inputs are connected AIN 1-5 and both sensors run off 3.3V, do I need an external Vref or is the internal generated reference sufficient?
3. I have tied RESET to DVDD and CLK to GND, what are you recommendations for remaining pins.
Thanks for your help thus far, I'm still a little green in this area so really appreciate the assistance.
Regards
Marc