Part Number: ADS1672
Hello,
I would like to know what are the single-ended electrical characteristics for the analog inputs, because in the datasheet only the typical values for differential mode and common mode are specified. I would like to know what are the single-ended requirements.
In particular, in my design the reference voltage Vref is +3V and the analog power supply AVDD is +5V. I would like to know if one of the inputs (either the positive or the negative side) can exceed Vref. Since in the absolute maximum ratings section it's stated that the "Analog I/O to AGND" should be between -0.3V and AVDD+0.3V, I would say that the inputs can exceed Vref as long as the voltage is less than AVDD, whereas Vref is only a reference for the differential voltage drop. But this is only a guess. I would like to know if it's true and if it can impair the performance.