This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC60508: DC output impedance affects Vout accuracy?

Part Number: DAC60508


Hello,

 

Datasheet specify DC output impedance, 0.085ohms(typ) with midscale output and 15ohms(typ) with DAC output at GND or Vdd.

Vout drops as follows due to the DC output impedance?

Vout = Vout target * load /( DC output impedance + load)

If so, DC output impedance varies depending on code, Vout drop voltage also varies depending on code?

My customer plans to drive 500ohms, and is concerned of Vout drop due to the DC output impedance.

Datasheet specifies only typical DC output impedance, but how much is the maximum DC output impedance?

 

Best regards,

 

K.Hirano