Other Parts Discussed in Thread: OPA365, LM1117
I've designed an circuit for a bio-medical application (university project). The adc input will be +or- 1V. Please verify if the circuit has any errors.
Microcontroller to be used- raspberry pi 4
* dvdd from micro controller
* avss,avdd from 3.7 v li-ion batteries connected to 2.5v voltage regulators,(+2.5,-2.5)
* Vref +2.048,-2.048 using ref5025.
* 1V differential input
schematic
https://drive.google.com/file/d/1KlNXJuF30Fy11g3TR3n-QaEXTD4h00b_/view?usp=sharing