Part Number: DAC70501
Other Parts Discussed in Thread: ADS7052, REF1925, REF1933
Hello,
I would like to use the 2.5V reference output from the DAC70501 to drive the analog supply input of the ADS7052 14b ADC. The ADS7052 data sheet recommends a 3.3uF cap at this input. Are there any concerns about loading the DAC70501 reference output with the 3.3uF cap? The ADS7052 analog supply current is specified at about 500uA, so I am guessing that this is a light enough load for the reference output.The specified load regulation of the reference is 90uV/mA, which is higher than a dedicated reference (such as the REF1925), but is still less than the LSB of the ADS7052.
Thanks,
Scott