Hi,
I am using an ADC 12 DJ 5200 RF mounted on a board I designed.
I use Xilinx XCKU15P-2FFVA1156E and ADC connected by JESD204B.
When a board is incorporated into a machine and operated, the JESD link is repeatedly broken and reconnected in no time.
This did not occur when the cooling fan was blowing on the evaluation bench, so it appears to be a cooling issue.
However, the temperature of the chip does not reach 80°C and the room temperature is about 20°C when viewed with a thermo-camera even when the chip is in the machine, so there does not seem to be such a problem.
Since there is little room in the machine, could you give me some ideas on how to deal with it other than adding a cooling mechanism?