Other Parts Discussed in Thread: ADS131A04
Hello,
I want to measure a high dynamic current (500nA to 60mA) using a shunt high side configuration with the ADS131A02. The common mode voltage will be between 1.8V and 3.6V. In the application, we need only a few tens of samples per second. DC accuracy is a must.
For this purpose, I will have 2 ranges, with 2 different shunts : 30 ohms and 3 kohms. The burden voltage of the shunt will be compensated thanks to an LDO. It means the ADC will be used in a pseudo-differential configuration where the AIN negative input will be held at a relatively constant voltage.
I know the ADC input differential impedance will change the gain of the whole chain, but I can calibrate it.
However I wonder what is the common mode leakage current of the inputs, and if it can be compensated by doing an offset calibration? Or do I need to put high impedance buffers between the inputs and the ADC?
Many thanks,
Victor