Part Number: ADS1259-Q1
Other Parts Discussed in Thread: ADS1259
Hi all,
Can you answer to the questions below about the settings to use this ADS1259-Q1 as single-ended setting (0-5V).
- To use full scale bits when setting AVDD=5V and AVSS=0V, how can I set VREFP and VREFN? If VREFP=5V and VREFN=2.5V, is ADS1259-Q1 able to use all 24 bits?
- What value should I put into FSC register in this case? I think gain is not needed for this and the default would be fine.
Thanks,
RYO