Part Number: DAC121S101
I am using the DAC121S101 to generate a sine wave.
The sine values are read form a lookup table, when writing the output very bad glitches can be seen on the output as shown below.
Using an analyzer I viewed the data being sent to the DAC which is shown below against a closer look at some of these glitches, the data does not appear to coincide with the glitch in the output of the DAC so I am relatively sure the error is caused within the DAC and the data being sent is OK. A snapshot of the error with the values being written to the DAC is below.
The DAC output here is the blue trace and the hex values represent the data being written to the DAC. these were recorded using the oscilloscope at the DAC pin. It's apparent that the data is continuously decreasing but the DAC output increases at times.
Other points to note, the power supply/reference voltage appears very clean and the SCLK frequency is 20MHz.
VA is +5V .
The circuit used below.
The output was measured at pin 4 of the DAC with capacitor C31 both populated and unpopulated and there was no change in behavior in the two cases.
Any assistance or guidance would be greatly appreciated.
Thanks!