This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS114S08B: ADS114S08B

Part Number: ADS114S08B


Hello,

I want to use the ADS114S08B as a 12 channel single ended ADC with PGA. The analog supply is +/- 2.5V (AVDD / AVSS), internal Vref, AINCOM = 0V (AGND).
The 12 analog voltages to be measured are between 0V and a maximum of -2V. There are no positive input voltages.
Are these measurements basically possible with the ADS114S08B?