Part Number: DAC7750
Hi team.
My customer is seeing the same input but different output.
The system load is 200Ω.
Ch1 : 17.2V(86mA)
Ch2 : 1.27V(6.8mA)
They are the circuits at output that referenced the data sheet(p.39 fig,62).
I have some question about this phenomenon.
1. Is this the output error?
Is the internal circuit damaged because the output is obviously high?
2. If it is the output error, Could you guess the cause of the error?
3. They were touching the wiring directly with a tester to check the output voltage.
Will it cause a malfunction?
Sincerely.
Kengo.