Part Number: DAC81416EVM
Hi,
Could you please confirm the current drawn from the power supply for DAC81416EVM? I didn't see any when it is connected:
VCC: positive 12 Volt
VSS: negative 12 Volt
Gnd: 0
Thanks.
Regards,
Andri
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DAC81416EVM
Hi,
Could you please confirm the current drawn from the power supply for DAC81416EVM? I didn't see any when it is connected:
VCC: positive 12 Volt
VSS: negative 12 Volt
Gnd: 0
Thanks.
Regards,
Andri
Hi Andri,
When you power up the EVM, device will be in power down mode and in this state it will draw only 20 to 30uA from VCC/VSS supply and I doubt you can measure that with a normal multi meter.
You need to write into the device to bring out of power down state and then you can start observing device supply current. When full code is loaded into device, you can expect 10 - 25mA of current depends on channel and output range.
Hope this helps.
Regards,
AK