Part Number: ADS8881
I have been unable to connect to my ADS8881EVMV2-PDK from the ADS8881 EVM software.
It appears to me that the board driver is OK - please see Device Manager image below.
The LED D2 is normally flashing rapidly. When I start the ADS8881 EVM software, it momentarily stops flashing rapidly a couple of times, then shows the 'Device Communication Error' from the image below, and continues flashing rapidly.
I have measured the supply voltage at the EEPROM IC, and it is 3V3 as expected.
I see a couple of bursts of activity on the SCL and SDA pins of the EEPROM IC while the program attempts to start.
I am running WIN10 Pro on the PC I have installed the EVM software on.
Any suggestions? Could it be a faulty ADC EVM board, or some other explanation ?
I don't have any other ADC EVM boards on hand to try with the PHI-EVM-Controller.