Part Number: ADS8866
Hi,
I am planning to use ADS8866 to achieve local sampling close to the sensor. Using daisy chain seemed to guarantee that the conversion will start at the same time for all sensors.
Based on the manual, this is not sure. It is mentioned that there is an internal clock for the ADC conversion and the SCLK is only for the serial operation. Thus, the conversion does not share the same clock.
I guess when the CONVST activates the conversion, the S/H saves the value at the S/H. Does the switch close to charge the hold capacitor in an internal clock event?
Is there any reset of the internal clock when the ADC starts the conversion via the CONVST pin?
Thanks in advance!