Other Parts Discussed in Thread: DAC8563, XTR300, TIPD155, DAC8760
We are considering using this chip in an IS (Intrinsically Safe) product design. We have the following issue with it:
We would have to supply about 21VDC to AVDD. IS rules allow them to short or open any pins of an IC internally. Given the dozen or so connections that need to be made to the DAC8750 to an internal 3.3V system which has lots of capacitance, it becomes unfeasible to protect all of those lines - prevent that capacitance from getting to the 21V which is fed into the hazardous area (to a HART instrument for example).
Have you run into this before and have a solution?
Mike.