Hi,
I'm doing a project that will use 8 ADS1299 to reach 64 EMG channels. I want to be able to configure each ADS separatelly, so I need cascaded mode, but I want to receive the samples of all ADS1299 like they are just one devide, so I need daisy chain mode.
I'm planning to connect all the ADS1299 in daisy chain configuration but with an independent CS pin to each device. When I want to write to a specific ADS, I just assert the respective CS pin and send the command. When I want to read registers or receive samples, I assert all ADS1299 CS pins, send the command and receive data in daisy chain mode.
It will work or I'm missing something?