This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC128S102QML-SP: 5962R0722701VZA package

Part Number: ADC128S102QML-SP

Hi Kirby / Team,

Does the 5962R0722701VZA  comes with formed pins or does the customer need to bend the device leads themselves ?

Regards,

Nir.

  • Hi Nir,

    If you download the datasheet or go into the "Ordering & quality" tab of the ADC128S102QML-SP product page on ti.com, you will see that the 5962R0722701VZA comes in the NAC package which has the leads already trimmed and formed.  The footprint matches that of a standard commercial plastic SOIC package.

    The "Z" in the product name indicates the NAC package.   It is also offered as 5962R0722701VFA, which is the NAD (flatpack) package which does require the leads to be trimmed and formed by the user.