Part Number: ADS1220
Hi ,
i'm working on a pt100 sensor project, and trying to interface the ADS1220 with microcontroller. In the datasheet, p4/74 of ADS1220, it is mentioned that the DOUT/(not)DRDY and DRDY pin should be active low, which means that it should be connected with Vcc and 10k resistance , then wire it with the microcontroller, but in some reference design (TIIDA-0095 ) these pins are connected directly ! it is confused,
Thank you in advance for your response. This is the schematic