Part Number: DAC60508
Other Parts Discussed in Thread: DAC80504, DAC81408
Hi there,
A few questions about the DAC60508:
- When writing to the LDAC bit in the trigger register, when exactly are the outputs updated with the contents of the buffer register? I imagine it's on the /CS rising edge after the write to the TRIGGER register but can't find confirmation of that in the datasheet.
- Is there any sort of "write and update all" functionality? I want to have all 8 outputs update simultaneously, but to different values, so I don't think BRDCAST is useful for me. Would I need to send eight register writes and then a 9th write to the TRIGGER register?
- Definitely wishing there were a hardware LDAC input... I need low-jitter updates and I think I can do that by using a hardware timer-counter on my uC to control when the rising edge of /CS happens, but it's a pain :P