Part Number: ADS1282EVM-PDK
Tool/software: Code Composer Studio
HELP!!!
I want to download my code into ads1282,so what software should i choose? Can ADCPro satisfy my eager?Or can keil?
Thanks
Evelyn
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Evelyn,
I'm afraid I'm not entire sure what you're asking for...
As part of the ADCPro connection process to the ADS1282EVM, the software will download/flash the MMB0 with the correct firmware so that you can use the EVM. If the EVM is connecting to ADCPro, then this process is working okay.
If you're asking about how to program an MCU to communicate with the ADS1282, then you would select the MCU and IDE of your choice to write the firmware for the MCU. The the ADS1282 is not a device that you would directly program; but you would typically program a microcontroller with a SPI peripheral to communicate with the ADC and modify the ADC's register values through SPI communication.