in the datasheet,1.8-V/3.3-V CMOS-Compatible Interface.i set IOVDD is 2.5V
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Yes, this is fine. As long as the CMOS IO such as FPGA interfacing with the DAC is also at 2.5V Level. You may use IBIS model for signal integrity simulation

You may also refer to figure 45 on the datasheet for the internal CMOS input structure with reference to IOVDD.
-Kang