Hi. I already posted several question about ADS5295. But I'm asking because there's still something I'm not sure about.
Q1. when I set 14x serialization mode and disable filter (like averaging..), where does two zero bit are added? to MSB? LSB?
for example 12bit (include information) is 111000111000 -> To LSB :111000111000+00
To MSB :00+111000111000 which one is correct?
Q2. When I set 14x serialization mode and sync pattern mode,
Two zero bit are added like question 1 (like (00)111111000000, 000000111111(00)?) or sync pattern become 11111110000000?
Thanks!