This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1298: lead off current setting for 500 M ohm DC impedance

Part Number: ADS1298

Hello,

We are using ADS1298IPAG in our design. As per datasheet section 7.5 Electrical Characteristics, DC input impedance during Current source lead-off detection mentioned as 500 M ohm. May I know this impedance specified is at which lead off current setting? As I understand lead off current can be set as 6nA,12nA,18nA and 24nA.

thanks

Shanoj