This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS131M04: Conversion start timing

Part Number: ADS131M04

Hi,

What is the trigger that the ADS131M04 starts conversion?

Best Regards,

Kuramochi

  • Kuramochi-san,


    The ADS131M04 starts conversions immediately after power-up of the device. This is shown in Figure 37 for Fast-Settling Behavior. However, you can also can see this in the State diagram showing the device functional modes in Figure 38. As the device powers up after a POR event or reset the device starts off in continuous conversion mode.

    However, if you need to trigger the start of a conversion, you can use the /SYNC/RESET pin. You would pull this pin to ground for a time shorter than 2047 tCLKIN (and longer than 1 tCLKIN). This starts a new conversion. You can read about this in the Synchronization in section 8.5.2.


    Joseph Wu