Hi,
I am using ADS130E08 as ADC in my project. if we read the datasheet its written that if VINP-VINN is greater than or equal to Vref then the digital output will be 7FFF.
in my application VINP(max):2.85V, VINN:1.65V, VIN(min):0.45V, Vref internal:2.4V, gain:2 with single ended mode
if I input 2.85V to the VINP, digital output is getting saturated at 72FA.
not getting full scale output during VINP:2.85V, is there any reason??
Thanks and regards
ARVINDA KUMAR