Other Parts Discussed in Thread: ADS5292, ADS5287
The interface type of ADS5282 is shown as "Parallel LVDS", while that of ADS5287 is shown as "Serial LVDS". However, from the datasheet, the internal structure of the two is the same, only the number of digits is different. ADS5292 is also shown as "Serial LVDS", but the interface mode is different from that of ADS5287 and ADS5282. The AD9222 interface mode of ADI is also defined as "Serial LVDS";
1. How do you define parallel LVDS and serial LVDS?
2. Is the interface type of ads5282 the same as that of ad9222? We want to replace ad9222 with ads5282
3. Is there any more suitable material to replace ad9222?