Part Number: DAC3162
Hi team,
My customer asked me a question about DAC3162. As a DDR input and DACA and DACB sample input are interleaved. The DACA data is latched at rising edge and DACB is latched at falling edge. However the datasheet does not explain at which edge the outputs are updated. If the output is updated at the same time when data is latched that will result phase delay between two channels. I searched for answer in forum and found same question was asked before. While it seems there is not final conclusion. (Some Tier said the two channels are updated at same time, however customer's test did not support this.)
Thank you!
John