Part Number: ADS127L01
Hello,
Our customer had built ES board and proceed to verify performance then they detect some aliasing noise spectrum as below.
We would like to get your advice how to achieve specified Digital Filter stop band attenuation level.
ADS127L01 setting:
HR mode
256kHz SPS
64OSR
DF WB2
Slave mode
Measurement result:
Input signal -1dBFS 156kHz sinewave
At 100KHz aliasing spectrum level is -90dB even WB2 stopband attenuation is 116dB.
Also, change input frequency to 166KHz
At 90KHz aliasing spectrum level is -87dB
Tried to shift frequency little bit but level is always stay around -87~90dB.
Regards,
Mochizuki