Part Number: ADS122C04
Other Parts Discussed in Thread: ADC-TEMP-SENSOR-FW, TPS734, ADS1248
For a new project we just started we have to measure temperatures between -180C and -160C with an accuracy <0.5C. Therefore we want to use a PT1000 (3- or 4 wire and class A or class B depending on the price). Probably our sensor supplier can deliver a PT1000 with 0.15C accuracy so we have 0.35C left for the ADC. Therefore some questions:
- Do you think an accuracy <0.35C is possible within this temperature range with the ADS122C04?
- The resistance of a PT1000 will be around 25 Ohm at -180C. Which reference resistor value would you suggest if we are only interested in accuracy around -180C? And which type of resistor would you recommend? I asume we have to set the IDAC value at max (1.5mA) to get enough voltage at this low sensor resistance value at very low temperature?
_ Do we have to implement the Callendar van Dussen equation in our software or can we just read the ADC value and calculate the temperature with that? I assume the sensor will be linear over such a small range?
- Are there any other things we have to take car for?
- I also found the LTC2986 which is very accurate but the price is very high for that part (and besides that one has SPI). So therefore the ADS122C04 could be an interesting part for us regarding the price.
Best Regards
Chris van der Aar
Sr. Hardware engineer
NTS Group
Eindhoven , The Netherlands