This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC12DJ3200: Recommended pressure

Part Number: ADC12DJ3200

Dear Technical Support Team,

Could you inform me of the recommended vertical pressure to the package(FCBGA)?

I concerned that the vertical pressure of the heat sink may damage ADC package.

The FCBGA(10mm x 10mm ) is much smaller than traditional packages,

so I guess that  the vertical pressure to fix the heat sink will concentrate and increase to the package.

According to the following E2E, it said that  IC is evaluated up to 100 [N]

Hi, This is the only data our packaging team has on this. "I found a FCBGA, Designator GTS, 23 X 23, 288 balls, 1.0mm pitch. Test stopped at 100N without failure." I recommend you either purchase…


ーーーーーーーーーーーーーーーーーーーーーーーーーー

This is the only data our packaging team has on this.

"I found a FCBGA, Designator GTS, 23 X 23, 288 balls, 1.0mm pitch. Test stopped at 100N without failure."

ーーーーーーーーーーーーーーーーーーーーーーーーーー

Best Reagrds,

ttd